Why is the MQ-pump switching off during operation?

It may be dry running; the suction line must be completely filled. The temperature of the media may be too high (> 35°C), the ambient temperature may be too high (> 45°C), the motor may be overloaded; check the pump shaft for free movement, the voltage supply may be too low, check the connection. Please consult a specialist company for such work.


    Facebook Twitter LinkedIn